Can LPC Link2 and MCUxpresso support MKL03Z32VFK4?

cancel
Showing results for 
Search instead for 
Did you mean: 

Can LPC Link2 and MCUxpresso support MKL03Z32VFK4?

196 Views
waynejeong
Contributor II

Hello 

I have made test board with MKL03Z32VFK4 and I am trying to download in MKL03Z32VFK4 on the board  using LPC link2 and MCUxpresso. But I can`t download firmware. 

Below is comment in console window 

=======================================================================================

DAP stride is 1024 bytes (256 words)
Inspected v.2 On chip Kinetis Flash memory module FTFA_1K_Tiny.cfx
Image 'Kinetis SemiGeneric Jul 7 2020 10:53:13'
Opening flash driver FTFA_1K_Tiny.cfx
Sending VECTRESET to run flash driver
Flash variant 'KL03 FTFA Generic 1K' detected (8KB = 8*1K at 0x0)
Closing flash driver FTFA_1K_Tiny.cfx
Connected: was_reset=true. was_stopped=true
Awaiting telnet connection to port 3331 ...
GDB nonstop mode enabled
GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.

=======================================================================================

Is it possible to download using LPC link2 and MCUxpresso?

If it can support it please, let me know what is problem.

Thank you.

0 Kudos
1 Reply

158 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Jeong,

LPC-Link2 has two firmware, CMSIS-DAP and Jlink. Both of them can support KL03. Please check

1. Have you install CMSIS-DAP or Jlink driver correctly

2. SWDIO pin need a pull-up resistor.

3. VDD power voltage

4. RESET pin and NMI pin. 

Please refer to https://www.nxp.com/webapp/Download?colCode=KLQRUG&location=null 

Regards,

Jing

0 Kudos