Hi Manva,
Base on the demo of "NfcrdlibEx10_MIFAREDESFire", Please add the following definitions in the APP_NxpBuild.h file:
#define NXPBUILD__PHAL_MFDFEV2_SW
#define NXPBUILD__PH_NDA_MFDFEV2
#define NXPBUILD__PHAL_VCA_SW
#define NXPBUILD__PH_TMIUTILS
and please also add the following definition in the file of "/NfcrdlibEx10_MIFAREDESFire/PN7462AU/phCommon/inc/ph_Status.h":
#define PH_COMP_TMIUTILS 0xE500U /**< TMI Utilities Code. */
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------