关于S32K144 IDE在WIN10下安装和运行的问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

关于S32K144 IDE在WIN10下安装和运行的问题

4,004 次查看
yangyongchao
Contributor I

我下载使用S32DS_ARM_Win32  V1.3 V2.0 R1三个版本,每个版本分别如下问题

1.3能正常安装,但是在使用SDO下载程序时提示问题,debug 设置界面里能找到设备,设备管理器驱动状态也正常

2.0版本双击安装文件后,让选择解压路径,选择解压路径后没有确定按钮,也不执行下一步

R1版本安装文件双击后,没有任何反应

以上安装,都有测试兼容的模式和管理员身份运行,结果一样

以上问题,有没有朋友遇到过

0 项奖励
8 回复数

3,678 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write your question in English? NXP support engineers are spread worldwide and official communication language is English.

Thank you for understanding.

Regards,

Martin

0 项奖励

3,678 次查看
yangyongchao
Contributor I

Thanks for your reply!

About S32DS_ARM_Win32  Three Versions,there are some questions in my computer,as follows:

1、V1.3,it runs  OK now, Before ,it cannot debug ,Because my project under the chinese path.

2、V2.0 ,Open the install files ,then shows the  uncompress path,after I select the path,there is not a button of "yes",so it cannot enter next step.

3、R1,Open the install ,then  there is  no response. This phenomenon may be relative to the java set.

so, I want to know how to deal with the questions 

0 项奖励

3,678 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

thank you for information. Could you please tell me which version of Java you use and also send me screen of the error you get during installation of S32DS 2018.R1?

Also, please be sure, you have administrator right for installation.

Regards,

Martin

0 项奖励

3,678 次查看
yangyongchao
Contributor I

pastedImage_1.pngJAVA Version 8,1.8.0_211-b12,the newest.

when I install the soft ,I tried Run as administrator,it is no efficient.

during installation of S32DS 2018.R1 ,there is not tips a error,No screen display!

thank you!

0 项奖励

3,678 次查看
liborukropec
NXP Employee
NXP Employee

Hello,

did you look into the windows "Event Viewer" if there's some error message related to the install? Theoretically there might be some clue.

Regards,

Libor

0 项奖励

3,678 次查看
yangyongchao
Contributor I

yeah,there must be something wrong with the file"ntdll.dll"

the windows  "Event Viewer" shows this,but I still do`t know how to deal with it .

pastedImage_1.png

pastedImage_2.png

0 项奖励

3,678 次查看
liborukropec
NXP Employee
NXP Employee

I do not know too. Try to google it, update OS. What you can also try is to switch temporarily to English locale, reboot and then try to install. I saw few cases when installers had problems with the Chinese locale.

Regards,

Libor

0 项奖励

3,678 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

if you cannot see any window during installation, it seems installation cannot be executed from some reason. I have already seen this issue once in my colleague's computer and only solution was reinstalling operating system.

Regards,

Martin

0 项奖励