keaz128 pins tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

keaz128 pins tools

1,534 Views
hervehuy
Contributor I

I am trying to implement a KEAZ128 (80pins) in a potential project but cannot use the existing pins tools.

 

So I am looking for a kinetis expert pins tools supporting KEAZ128 microprocessor.

Labels (1)
2 Replies

1,250 Views
hervehuy
Contributor I

Hi Carlos,

I installed the Kinetis Studio Design tool provided here: Kinetis Design Studio Integrated Development Enviro|NXP

And I have been able to use the processor pin tools embedded.

Thanks !

1,250 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Herve,

Unfortunately the KEAZ devices are not supported by KSDK so the Pins Tool is not available for them, as an alternative you can use Processor Expert, here is a post created by a colleague that gives an overview of this tool:

https://mcuoneclipse.com/2015/10/18/overview-processor-expert/

Here is also a post where the Pins Tool and Processor Expert are compared:

https://mcuoneclipse.com/2016/06/08/tutorial-muxing-with-the-new-nxp-pins-tool/

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------