.ahbBusTimeoutCycle incorrectly generated

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

.ahbBusTimeoutCycle incorrectly generated

1,568 次查看
barrett_lowe
Contributor II

In the config tools the .ahbBusTimeoutCycle value is generated incorrectly in the final .c file. It seems like it mirrors the .ahbGrantTimeoutCycle value. As I change it in the peripheral tool UI, the generated code does not change. You can see in the screenshot attached, the code on the right does not reflect the value in the UI. Regenerating the code does not help.

I am using an i.MXRT1064 chip with v7.0 of the config tools. 

标记 (3)
0 项奖励
回复
2 回复数

1,450 次查看
Lukas_Heczko
NXP Employee
NXP Employee

Hi Barrett,

Thank you for reporting this issue. Attached you can find patch fixing this issue. The problem will be fixed also in the next update of MCUXpresso Config Tools v7.

Installation steps:

  1. Ensure you have an administrator rights, MCUXpresso Configuration Tools are not running and the MCU data of the MCUs you want to use are available (downloaded) on your desktop.
  2. Copy the content of this archive into the tool's data folder:
    Windows: c:\ProgramData\NXP\mcu_data_v7
    Linux/Mac: /home/<USER>/.nxp/mcu_data_v7

Regards,

Lukas

0 项奖励
回复

1,450 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Barrett,

The picture is deleted by system. Would you mind resend it?

Regards,

Jing

0 项奖励
回复