Why does MCUXpresso Config tool limit i.MX to only the RT1052

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why does MCUXpresso Config tool limit i.MX to only the RT1052

ソリューションへジャンプ
2,496件の閲覧回数
tbiberdorf
Contributor IV

I've installed MCuXpresso Config Tools Versino 11.0

tbiberdorf_0-1649342110173.png

and I'm attempting to start a new configuration: File->New -> Create a new configuration

tbiberdorf_1-1649342202485.png

I select the Create a new standalone configuration for processor, board or kit

tbiberdorf_2-1649342270772.png

and the only i.MX RT allowed to choose from is the MIMXRT1052.

 

How do I get this utility to allow ALL the i.MX controllers?

 

Thanks

0 件の賞賛
返信
1 解決策
2,489件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi, 

As you can see the exclamation mark and message in the top-left part of the dialog, the tool is not able to access the network. Config tools need internet connection to access the list of the processors and download additional data for the selected processor.

Do you have the internet connection available on the machine? 

If the problem persists, please take a look in this thread: https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team

元の投稿で解決策を見る

4 返答(返信)
2,459件の閲覧回数
tbiberdorf
Contributor IV

Thanks.  I down loaded the RT1062 support file and now I can review/modify the .mex file!

0 件の賞賛
返信
2,476件の閲覧回数
tbiberdorf
Contributor IV

Hi Petr

This message is very confusing to me, as I definitely have internet connection, As I just downloaded the on-line install .exe and installed the application.  I also have a connection to this forum to post this message to.

0 件の賞賛
返信
2,469件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi,

most probably it will be the proxy/antivirus with proxy.

Could you please post here log file %USERPROFILE%/.nxp/swtools.log

Thank you,

Libor

0 件の賞賛
返信
2,490件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi, 

As you can see the exclamation mark and message in the top-left part of the dialog, the tool is not able to access the network. Config tools need internet connection to access the list of the processors and download additional data for the selected processor.

Do you have the internet connection available on the machine? 

If the problem persists, please take a look in this thread: https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team