Why does MCUXpresso Config tool limit i.MX to only the RT1052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does MCUXpresso Config tool limit i.MX to only the RT1052

Jump to solution
2,497 Views
tbiberdorf
Contributor IV

I've installed MCuXpresso Config Tools Versino 11.0

tbiberdorf_0-1649342110173.png

and I'm attempting to start a new configuration: File->New -> Create a new configuration

tbiberdorf_1-1649342202485.png

I select the Create a new standalone configuration for processor, board or kit

tbiberdorf_2-1649342270772.png

and the only i.MX RT allowed to choose from is the MIMXRT1052.

 

How do I get this utility to allow ALL the i.MX controllers?

 

Thanks

0 Kudos
Reply
1 Solution
2,490 Views
Petr_H
NXP Employee
NXP Employee

Hi, 

As you can see the exclamation mark and message in the top-left part of the dialog, the tool is not able to access the network. Config tools need internet connection to access the list of the processors and download additional data for the selected processor.

Do you have the internet connection available on the machine? 

If the problem persists, please take a look in this thread: https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team

View solution in original post

4 Replies
2,460 Views
tbiberdorf
Contributor IV

Thanks.  I down loaded the RT1062 support file and now I can review/modify the .mex file!

0 Kudos
Reply
2,477 Views
tbiberdorf
Contributor IV

Hi Petr

This message is very confusing to me, as I definitely have internet connection, As I just downloaded the on-line install .exe and installed the application.  I also have a connection to this forum to post this message to.

0 Kudos
Reply
2,470 Views
liborukropec
NXP Employee
NXP Employee

Hi,

most probably it will be the proxy/antivirus with proxy.

Could you please post here log file %USERPROFILE%/.nxp/swtools.log

Thank you,

Libor

0 Kudos
Reply
2,491 Views
Petr_H
NXP Employee
NXP Employee

Hi, 

As you can see the exclamation mark and message in the top-left part of the dialog, the tool is not able to access the network. Config tools need internet connection to access the list of the processors and download additional data for the selected processor.

Do you have the internet connection available on the machine? 

If the problem persists, please take a look in this thread: https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-a...

Regards

Petr Hradsky

Config Tools Team