Using config tools to set up a composite USB for HID and CDC VCOM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using config tools to set up a composite USB for HID and CDC VCOM

1,640 Views
JJ_93
Contributor I

I am using the LPC54S018J4M

I have my code set up and working for USB HID, but I want to add in the ability to make it composite so I can include CDC VCOM as well for additional data I am getting elsewhere. My question is am I able to use the config tools/USB config in some way so I can get a general framework for the code and then I will edit it as I need? I just basically want to know if there is an easier way to do this than coding it from scratch.

Any help would be much appreciated

Tags (3)
0 Kudos
Reply
1 Reply

1,621 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

The Configure tool doesn't support lpc54s018 USB so far, recommend refer to the USB demos under SDK.

 

BR

Alice

0 Kudos
Reply