Unable to find ADC peripheral for MKE04Z8VWJ4 in MCUXpresso.

cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to find ADC peripheral for MKE04Z8VWJ4 in MCUXpresso.

931 Views
manisht_24
Contributor II

Dear Members,

        I am Using MCUXpresso to write a code for MKE04Z8VWJ4 part and I want to use 2 pins as an ADC.

I have selected ADC as pin function for PTA1 and PTA0 from pin configuration. 

        Actually I want to generate ADC interrupt but couldn't find ADC in Peripherals list ( Image attached ).

Can you guide me how to Create ADC configuration and how to write a code to measure ADC voltage? 

Regards.

0 Kudos
1 Reply

901 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @manisht_24 ,

 

The MCUXpresso Config Tool doesn’t support KE04 with peripheral config for the ADC, however you can use an example from a K06 that contains ADC examples on the SDK in order to use it as a guide (guide only) for the ADC configuration, taking on a count that some register values will defer so also while looking on the example have you reference manual for KE04 in order to verify register values.

 

Reference Manual KE04

https://www.nxp.com/webapp/Download?colCode=MKE04P80M48SF0RM

0 Kudos