When the controller was running , I touch the power chips to know the heating, then SPC5668G suddenly not run . Later I find the flash can’t be erased by BDM and IC5000. The software can’t be download. How can I do next?
Hello,
could you please write me, if you use LQFP or BGA package? Also I need to know, if you have soldered the microcontroller or if you use socket.
It is also possible that you destroyed the microcontroller using static charge. At first, please measure reset line and in case reset line is always 0, microcontroller is destroyed. It is also possible that only some part of microcontroller is damaged and this could be the reason you are not able to connect.
Regards,
Martin
Hi Yp Chang,
MCUXpresso Config Tools supports Cortex-M Kinetis and LPC devices. MPC devices are not supported.
I'd recommend to submit this question to MPC related comunity: https://community.nxp.com/community/s32/mpc5xxx
Regards
Marek