MCUExpresso Config tool and RT1064 SEMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUExpresso Config tool and RT1064 SEMC

Jump to solution
2,814 Views
randyhermes
Contributor III

If there a way to configure the RT1064 SEMC SRAM mode in the MCUExpresso Config Tool?

When you select the SEMC it only allows the SDRAM interface to be configured.

According to the processor reference manual region 6 of the SEMC is used for the SRAM interface.

I would like to use this feature to interface to an external FPGA.

Randy

0 Kudos
Reply
1 Solution
2,786 Views
randyhermes
Contributor III

Hi Adrian,

Thanks for letting me know.  Are there any plans to expand SEMC configuration support in future versions?

Randy

View solution in original post

0 Kudos
Reply
3 Replies
2,787 Views
randyhermes
Contributor III

Hi Adrian,

Thanks for letting me know.  Are there any plans to expand SEMC configuration support in future versions?

Randy

0 Kudos
Reply
2,779 Views
addiyi
NXP Employee
NXP Employee

Hi Randy,

We plan to support all SEMC interfaces in the next releases.

Thanks,

Adrian

0 Kudos
Reply
2,797 Views
addiyi
NXP Employee
NXP Employee

Hi Randy,

Currently only SEMC/SDRAM is supported in MCUXpresso Config Tools.

Adrian

0 Kudos
Reply