LPC55S69 - GPIO Pin as NMI using Config Tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S69 - GPIO Pin as NMI using Config Tools

跳至解决方案
2,296 次查看
PhilV
Contributor III

Hi, I am using mcuXpresso with the config tool to setup an LPC55S69.

I want PIO1_18 to be non-maskable-interrupt.
In the user manual for the LPC55S69 it seems to indicate that this is possible, but I do not see how to do this via the configuration tools?

In the Pin Configuration "Pins" table I have set it for "PINT:PINT,0" (do I also need to set it as GPIO?)

In the Peripherals Configuration tool I can then configure the PINT for Falling edge etc.
I can also choose to "Enable callback/interrupt" - (what is the reason for being able to configure it and not enable it?)
If I enable it I can then name a callback function and handle it... but I don't see any option to make this the NMI? 

Please advise?

0 项奖励
回复
1 解答
2,267 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @PhilV 

Config tools is usefull for some "simple" configurations and it does not supports all the modules, since the SYSCON is something more complicated besides the clocks configurations and the NMI setup has to be by writing on the register by programming them.

Best Regards, Miguel.

在原帖中查看解决方案

2 回复数
2,171 次查看
PhilV
Contributor III

Just for future visitors... 

See also this thread for the implementation details:

https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-IRQ-Numbers-for-NMI/m-p/1723892/highlight...

2,268 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @PhilV 

Config tools is usefull for some "simple" configurations and it does not supports all the modules, since the SYSCON is something more complicated besides the clocks configurations and the NMI setup has to be by writing on the register by programming them.

Best Regards, Miguel.