LPC5512 USB use is in conflict with the data sheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5512 USB use is in conflict with the data sheet

ソリューションへジャンプ
3,614件の閲覧回数
randylee
Contributor V

I'm using MCUExpresso 11.2.0 and Config Tools 8.0 and SDK 2.8  I'm laying out a board with an LPC5512JBD64 on it.  Looking at the pins tool and the datasheet for this part from Rev 1.0 3-March 2020 (LPC55S1X/LPC551X)

The pins tool says that USB0 (pins 61-64) can be connected but not USB1 (pins 22-27) which it enforces!

The datasheet says that USB1 can be connected but USB0 is unconnected on this part.

One of these is wrong but with only 2 data points, I have no idea which one.  I'm hoping it's the data sheet because the pins tool won't LET me do it the way the datasheet wants it done.

ラベル(1)
1 解決策
3,511件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Randy, I hope you're doing well!

 

The LPC5512 variant of the LPC551x only has the Full-Speed USB controller available, which corresponds to USB0:

pastedImage_3.png

(Taken from the LPC55S1x Datasheet, table 2).

 

Still, the USB1 High-Speed controller is available on the other variants of the LPC551x.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,511件の閲覧回数
randylee
Contributor V

OK, so the tools are right, USB0 is the one that's active....  at least according to Table 2....

But on page 36 of that datasheet the pinouts show:

pastedImage_1.png

so I'm thinking that this is a datasheet error?

thanx

0 件の賞賛
返信
3,511件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Randy,

 

Thank you very much for your feedback!

 

We will be taking a look at this table in the documentation to provide a fix in a future release.

Please let me know if you need any more information.

 

Best regards,

Sebastian

3,512件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Randy, I hope you're doing well!

 

The LPC5512 variant of the LPC551x only has the Full-Speed USB controller available, which corresponds to USB0:

pastedImage_3.png

(Taken from the LPC55S1x Datasheet, table 2).

 

Still, the USB1 High-Speed controller is available on the other variants of the LPC551x.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信