Hello,
i want to use an 10Mhz external clock from an Oszillator.
System clock shall be 120Mhz.
( by the way the data sheet says up to 150Mhz , manual UM10914 says 100Mhz )
I want to feed the flexcoms with the pll and not with the fro.
But i can't use the tool for that.
FRGCLKSEL to pll_clk will lead to the only option *256, which in my opinion is nonsense!
Error Message :
Issue: Output frequency must be lower than or equal to: 48 MHz
Level: Error
Type: Tool problem
Tool: Clocks
Origin: Clocks: BOARD_BootClockRUN
Resource: SYSCON.FRGCTRL_DIV
Information: Output frequency must be lower than or equal to: 48 MHz (See constraint 1)