Error in Config Tools for FlexCAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in Config Tools for FlexCAN

Jump to solution
2,379 Views
stefano-quantic
Contributor III

In: Config Tools | Peripherals | Peripheral drivers (device specific) | FLEXCAN | Flexcan general configuration | FlexCAN configuration

there is a setting named "Self Reception" (the 14th settings of this block; it's a checkbox).
It should be renamed "Disable Self Reception", since its value determines the value of flexcan_config_t.disableSelfReception in the generate code (in peripherals.c), which in turn determines the setting for FlexCAN's bit MCR[SRXDIS].
The current name suggests the exact opposite of what it does, so it's very confusing.

This is for a project using iMXRT1176.

0 Kudos
Reply
1 Solution
2,311 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting the issue. You are right that the name of the setting is confusing and should be fixed.

I have already created a ticket to fix the issue in the next release of MCUXpresso Config Tools.

Best Regards,

Marek Neuzil

View solution in original post

0 Kudos
Reply
1 Reply
2,312 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Thank you for reporting the issue. You are right that the name of the setting is confusing and should be fixed.

I have already created a ticket to fix the issue in the next release of MCUXpresso Config Tools.

Best Regards,

Marek Neuzil

0 Kudos
Reply