MCUXpresso IDE v11.0.1 [Build 2563] [2019-09-01]
SDK_2.6.0_MKV31Fyyyxxx12.zip
where yyy is either 512 or 256.
both sdk's are version 228 2019-06-14
both sdk's are manifest 3.5.0
The 256 processor variant produces the following warning/error when the Peripherals Config tool is selected:
Device Configuration tool does not support selected processor. Select different tool.
The 512 variant did not exhibit the problem. Partial screen shot attached. Please advise on how to remedy this.
解決済! 解決策の投稿を見る。
Hi David,
Unfortunately, this device is not supported by the Peripherals Config Tool. You can check which devices are supported by the MCUXpresso Tools in the following link.
https://community.nxp.com/docs/DOC-333073
Hope it helps!
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi David,
good news is that MKV31F256xxx12 will be supported by Peripherals tool in MCUXpresso Config Tools v7 released at the end if this year.
Regards,
Lukas
Excellent. Thank you for the timely reply and clarity.
Hi David,
Unfortunately, this device is not supported by the Peripherals Config Tool. You can check which devices are supported by the MCUXpresso Tools in the following link.
https://community.nxp.com/docs/DOC-333073
Hope it helps!
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------