Corrupted archive on MCUXpresso Config tools download.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Corrupted archive on MCUXpresso Config tools download.

Jump to solution
3,294 Views
andrewparlane2
Contributor III

I'm trying to install the desktop MCUXpresso config tools, but windows claims the download is corrupted (6 times, over two days).

 

Details:

download page: Software Development Kit for Kinetis MCUs|NXP

file: Kinetis Expert Pins Tools V2.0, Windows 64bit package, offline installer(REV 2.0)

OS: windows 10 pro 64 bit

browser: Chrome - Version 53.0.2785.116 m + Internet Explorer - Version 11.447.14393.0

logged in to NXP state: both not logged in, and logged in.

 

Every downloaded file is 100 MB (104,857,600 bytes)

They contain exactly the same data.

On opening the .exe - windows says "Windows protected your PC, Windows smart screen prevented an unrecognised application from running. Running this application may put your PC at risk. application 'Kinetis_Expert_Configuration_Tools_v2_x64_offline_b161010 (2).exe'

After pressing "run anyway" I get "Error: This archive is corrupted".

Labels (1)
0 Kudos
Reply
1 Solution
2,657 Views
liborukropec
NXP Employee
NXP Employee

Hello,

the problem is being investigated, apparently it is problem for European users. Please try to use the online installer (available when you show "More" on the mentioned download page.

http://www.nxp.com/assets/downloads/data/en/software/Kinetis_Expert_Configuration_Tools_v2_x64_onlin... 

It should work for you.

Regards,

Libor

View solution in original post

4 Replies
2,658 Views
liborukropec
NXP Employee
NXP Employee

Hello,

the problem is being investigated, apparently it is problem for European users. Please try to use the online installer (available when you show "More" on the mentioned download page.

http://www.nxp.com/assets/downloads/data/en/software/Kinetis_Expert_Configuration_Tools_v2_x64_onlin... 

It should work for you.

Regards,

Libor

2,657 Views
andrewparlane2
Contributor III

Hi Libor,

Thanks, that's great. The online installer worked fine. I hadn't noticed that.

Andy

0 Kudos
Reply
2,657 Views
MarekTrmac
NXP Employee
NXP Employee

Hi Andy,

it seems the issue was resolved and offline installer can be downloaded. Sorry for inconvenience.

Regards

Marek

0 Kudos
Reply
2,657 Views
andrewparlane2
Contributor III

This still appears to be happening several days later.

I have tried both in the office and at home, on two separate machines now.

In the UK for reference.

0 Kudos
Reply