cancel
Showing results for 
Search instead for 
Did you mean: 

Overview of using the MIMXRT1170-EVK with MCUXpresso IDE

lpcxpresso_supp
NXP Employee
NXP Employee
0 1 133

Please find attached a document detailing various features related to using the iMXRT1170-EVK evaluation board with MCUXpresso IDE v11.3.x and SDK v2.9, including details of multicore debugging on this MCU.

 

Yours,

MCUXpresso IDE Support

1 Comment
jeremyzhou
NXP TechSupport
NXP TechSupport

Hi @Childe,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd like to know more information about your issue, so I hope you can answer the below inquires.
1) Is the first time to debug the MIMXRT1170-EVK board?
1.1) If not, did the phenomenon happen before?
1.2) If yes, did you ever change the hardware setting of the board or not?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------