Overview of using the MIMXRT1060(4)-EVK with MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overview of using the MIMXRT1060(4)-EVK with MCUXpresso IDE

lpcxpresso_supp
NXP Employee
NXP Employee
2 0 7,402

Updated v1.02  1st March 2019

 

Please find attached a document detailing various features related to using the iMXRT1060-EVK evaluation board with MCUXpresso IDE v10.3.x and SDK v2.5, including details of how to enable SWO trace on this MCU.

 

Updated to include a section on the MIMXRT1064 EVK.

 

Also attached are:

 

  • an example project demonstrating how SWO trace features may be enabled
  • an updated LinkServer (CMSIS-DAP) flash driver for the iMXRT1064 containing a fix for Mass Erase

 

Yours,

 

MCUXpresso IDE Support