cancel
Showing results for 
Search instead for 
Did you mean: 

New MCUXpresso Software Releases Now Available

nxf46154
NXP Employee
NXP Employee
0 2 1,233

New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available. In addition to new product support, you will find these updates and enhanced features in the new releases:

MCUXpresso SDK v2.6.0

  • Updated peripheral drivers to v2.6.0 SDK code base for all included boards and devices
  • Updated to latest GNU Arm Embedded Toolchain to GCC8 (2018-q4-major)
  • Expanded device and board support for Cypress Wi-Fi, nghttp2 (HTTP/2)
  • Inclusion of MQX v5.x Application Builder
  • Updated included middleware –
    • Amazon FreeRTOS Kernel v1.4.7+
    • Arm Mbed TLS v2.13.1
    • IwIP v2.1.2
    • Microsoft Azure Cloud Connectivity SDK v1.2.13
    • TensorFlow Lite and ARM CMSIS-NN (eIQ™ ML Software)
    • Segger emWin 5.48r
  • Updates to NXP developed middleware - USB Stack

MCUXpresso IDE v11.0.0

  • Improved support for Cortex-M33 secure / non-secure projects
  • Updated underlying Eclipse Framework to 4.10.0v201812 / CDT 9.6.0
  • New “Heap and Stack Usage” view provides ability to track heap and stack usage during debug of baremetal projects
  • Implemented “editor awareness” for linker map files, linker scripts and linker script templates, providing syntax coloring as well as navigation of file contents
  • New “Image Info” view gives a breakdown analysis of a project build, including overall memory usage, content of memory regions and static call graph (including stack usage information)
  • FreeRTOS Task Aware Debugging functionality now directly implemented within the IDE

   Learn more by reading this IDE Blog Article.

MCUXpresso Config Tools v6.0

  • Addition of Trusted Execution Environment (TEE) tool supporting Cortex-M33 TrustZone
  • Addition of Device Configuration tool, supports Device Configuration Data (DCD) commands configuration
  • Code changes are graphically tracked in real-time within the code preview window
  • Project Cloner in New Configuration Wizard: Added support for MCUXpresso SDK v2.6
  • Peripherals Tool: Documentation view history can now be navigated
  • ‘Update Code’ now possible without an assigned toolchain project
Tags (1)
2 Comments
dav1
Contributor V

nxf46154

Any chance to get a more detailed change-note list (or even better, the git commit history) for what has been changed from 2.5 -> 2.6

  • Updated peripheral drivers to v2.6.0 SDK code base for all included boards and devices

Also wonder what was fixed in the "USB Stack updates
 

lucasrangit
Contributor III

dav1‌ You can find that in the SDK DOCs archive (separate download). For my MCU, there's a release note with the detailed change log for each version.

For example, for USB in "MCUXpresso SDK Release Notes Supporting FRDM-K22F, TWR-K22F120M, and USB-KW41Z-K22F" I have the following. Check the SDK manifest to know what version of the driver is included.

USB stack for MCUXpresso SDK
The current version of USB stack is 2.2.0.
• 2.2.0
– New features:
* Added device DFU support.
* Supports OM13790DOCK on LPCXpresso54018.
* Added multiple logical unit support in MSC class driver, updated usb_device_lba_-
information_struct_t to support this.
* Supports multiple transfers for host ISO on IP3516HS.
– Bug fixes:
* Fixed device ip3511 prime data length than maxpacket size issue.
* Initialized interval attribute in usb_device_endpoint_struct_t/usb_device_endpoint_-
init_struct_t.
* Removed unnecessary header file in device CDC class driver, removed unnecessary usb-
_echo, and added DEBUG macro for necessary usb_echo in device CDC class driver.
* Fixed device IP3511HS unfinished interrupt transfer missing issue.