cancel
Showing results for 
Search instead for 
Did you mean: 

MCUXpresso Config Tools v6 Now Available

NXP Employee
NXP Employee
1 0 364

We are pleased to announce that MCUXpresso Config Tools v6 are now available.

 

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

Features

  • Available as Web, Desktop application and MCUXpresso IDE plug-ins
  • MCUXpresso SDK v2 support
  • Multicore support
  • GUI localized for English and Simplified Chinese
  • Mostly Connected: On-Demand device data download
  • Integrates with any compiler and IDE
  • Currently there are the following tools available: 

    MCUXConfigTools_BD.jpg

Downloads

 

Overview of Changes - version 6

  • Only 64bit operating systems supported.
  • 'Update Code' now possible without an assigned toolchain project.
  • Removed dialog reporting changes between MEX and YAML in source code. The changes can be reviewed using Update Code DIFF.
  • Added "Help | Processor Information" menu option displays information about currently used processor.
  • Added Device Configuration tool, supports DCD (Device Configuration Data) commands configuration.
  • Added Trusted Execution Environment (TEE) tool.
  • Highlight changes implemented in generated code in Code preview view.
  • (MCUXpresso IDE only): Added Dark theme support
  • (MCUXpresso IDE only): Added SEMC (SDRAM) Validation tool, with RT1020 and RT1050 support.
  • Project Cloner in New Configuration Wizard: Added support for MCUxpresso SDK v2.6.x
  • Clocks tool: Run Mode and MCG Mode selection have been moved to Clocks Diagram and Clocks Table views.
  • Clocks tool: Added support for search by label in Clocks Diagram.
  • Peripherals tool: Added Support for 64bit (and more) values from user.
  • Peripherals tool: User can now migrate settings values from component already added to a configuration to another component, if mutually compatible (component redesigned etc.).
  • Peripherals tool: Documentation view history can now be navigated.
  • (MCUXpresso Config Tools only): Added Overview dialog on opening configuration for the first time 


Community

MCUXpresso Config Tools

 

 

MCUXpresso Config Tools Data

The Data for MCUXpresso Config Tools v6 was successfully deployed on the production system.

 

What’s new in data

The Data for MCUXpresso Config Tools v6 release provides following updates:

  1. Update of all supported processors data to support new features introduced in MCUXpresso Config Tools v6
  2. Update of Peripherals tool components to support SDK Release 10
  3. Various bug fixes and improvements

 

Supported processors, boards, kits and components

 

Processors:

KinetisKinetis2LPCi.MXOther
MK02FN128xxx10MKE18F256xxx16LPC51U68MCIMX7U3xxxxxGenericMQX
MK02FN64xxx10MKE18F512xxx16LPC54005MCIMX7U5xxxxxQN908XC
MK10DN512xxx10MKL02Z16xxx4LPC54016MIMX8MD6xxxHZ
MK10DX128xxx10MKL02Z32xxx4LPC54018MIMX8MD6xxxJZ
MK10DX256xxx10MKL02Z8xxx4LPC54101J256MIMX8MD7xxxHZ
MK11DN512Axxx5MKL03Z16xxx4LPC54101J512MIMX8MD7xxxJZ
MK11DN512xxx5MKL03Z32xxx4LPC54102J256MIMX8MM1xxxKZ
MK11DX128Axxx5MKL03Z8xxx4LPC54102J512MIMX8MM1xxxLZ
MK11DX128xxx5MKL13Z32xxx4LPC54113J128MIMX8MM2xxxKZ
MK11DX256Axxx5MKL13Z64xxx4LPC54113J256MIMX8MM2xxxLZ
MK11DX256xxx5MKL14Z32xxx4LPC54114J256MIMX8MM3xxxKZ
MK12DN512xxx5MKL14Z64xxx4LPC54605J256MIMX8MM3xxxLZ
MK12DX128xxx5MKL15Z128xxx4LPC54605J512MIMX8MM4xxxKZ
MK12DX256xxx5MKL15Z32xxx4LPC54606J256MIMX8MM4xxxLZ
MK20DN512xxx10MKL15Z64xxx4LPC54606J512MIMX8MM5xxxKZ
MK20DX128xxx10MKL16Z128xxx4LPC54607J256MIMX8MM5xxxLZ
MK20DX256xxx10MKL16Z256xxx4LPC54607J512MIMX8MM6xxxKZ
MK21DN512Axxx5MKL16Z32xxx4LPC54608J512MIMX8MM6xxxLZ
MK21DN512xxx5MKL16Z64xxx4LPC54616J256MIMX8MQ5xxxHZ
MK21DX128Axxx5MKL17Z128xxx4LPC54616J512MIMX8MQ5xxxJZ
MK21DX128xxx5MKL17Z256xxx4LPC54618J512MIMX8MQ6xxxHZ
MK21DX256Axxx5MKL17Z32xxx4LPC54628J512MIMX8MQ6xxxJZ
MK21DX256xxx5MKL17Z64xxx4LPC54S005MIMX8MQ7xxxHZ
MK21FN1M0Axxx12MKL24Z32xxx4LPC54S016MIMX8MQ7xxxJZ
MK21FN1M0xxx12MKL24Z64xxx4LPC54S018MIMXRT1015xxxxx
MK21FX512Axxx12MKL25Z128xxx4LPC55S66MIMXRT1021xxxxx
MK21FX512xxx12MKL25Z32xxx4LPC55S69MIMXRT1051xxxxB
MK22DN512xxx5MKL25Z64xxx4LPC802MIMXRT1052xxxxB
MK22DX128xxx5MKL26Z128xxx4LPC804MIMXRT1061xxxxA
MK22DX256xxx5MKL26Z256xxx4LPC810MIMXRT1062xxxxA
MK22FN128xxx10MKL26Z32xxx4LPC811MIMXRT1064xxxxA
MK22FN128xxx12MKL26Z64xxx4LPC812
MK22FN1M0Axxx12MKL27Z128xxx4LPC822
MK22FN1M0xxx12MKL27Z256xxx4LPC824
MK22FN256xxx12MKL27Z32xxx4LPC832
MK22FN512xxx12MKL27Z64xxx4LPC834
MK22FX512Axxx12MKL28Z512xxx7LPC844
MK22FX512xxx12MKL33Z128xxx4LPC845
MK24FN1M0xxx12MKL33Z256xxx4LPC8N04
MK24FN256xxx12MKL33Z32xxx4
MK26FN2M0xxx18MKL33Z64xxx4
MK27FN2M0Axxx15MKL34Z64xxx4
MK27FN2M0xxx15MKL36Z128xxx4
MK28FN2M0Axxx15MKL36Z256xxx4
MK28FN2M0xxx15MKL36Z64xxx4
MK30DN512xxx10MKL43Z128xxx4
MK30DX128xxx10MKL43Z256xxx4
MK30DX256xxx10MKL46Z128xxx4
MK40DN512xxx10MKL46Z256xxx4
MK40DX128xxx10MKL82Z128xxx7
MK40DX256xxx10MKM34Z256xxx7
MK50DN512xxx10MKS20FN128xxx12
MK50DX256xxx10MKS20FN256xxx12
MK51DN256xxx10MKS22FN128xxx12
MK51DN512xxx10MKS22FN256xxx12
MK51DX256xxx10MKV10Z128xxx7
MK52DN512xxx10MKV10Z16xxx7
MK53DN512xxx10MKV10Z32xxx7
MK53DX256xxx10MKV10Z64xxx7
MK60DN256xxx10MKV11Z128xxx7
MK60DN512xxx10MKV11Z64xxx7
MK60DX256xxx10MKV30F128xxx10
MK63FN1M0xxx12MKV30F64xxx10
MK64FN1M0xxx12MKV31F128xxx10
MK64FX512xxx12MKV31F256xxx12
MK65FN2M0xxx18MKV31F512xxx12
MK65FX1M0xxx18MKV42F128xxx16
MK66FN2M0xxx18MKV42F256xxx16
MK66FX1M0xxx18MKV42F64xxx16
MK80FN256xxx15MKV44F128xxx16
MK82FN256xxx15MKV44F256xxx16
MKE02Z16xxx4MKV44F64xxx16
MKE02Z32xxx4MKV46F128xxx16
MKE02Z64xxx4MKV46F256xxx16
MKE04Z128xxx4MKV56F1M0xxx24
MKE04Z64xxx4MKV56F512xxx24
MKE04Z8xxx4MKV58F1M0xxx24
MKE06Z128xxx4MKV58F512xxx24
MKE06Z64xxx4MKW21D256xxx5
MKE14F256xxx16MKW21D512xxx5
MKE14F512xxx16MKW21Z256xxx4
MKE14Z128xxx7MKW21Z512xxx4
MKE14Z256xxx7MKW22D512xxx5
MKE14Z32xxx4MKW24D512xxx5
MKE14Z64xxx4MKW31Z256xxx4
MKE15Z128xxx7MKW31Z512xxx4
MKE15Z256xxx7MKW35A512xxx4
MKE15Z32xxx4MKW35Z512xxx4
MKE15Z64xxx4MKW36A512xxx4
MKE16F256xxx16MKW36Z512xxx4
MKE16F512xxx16MKW41Z256xxx4
MKE16Z32xxx4MKW41Z512xxx4
MKE16Z64xxx4

 

Boards
FRDM-K22FHVP-KV11Z75MMIMX8QM-MEK-REV-B
FRDM-K28FHVP-KV31F120MMIMX8QX-MEK-REV-B
FRDM-K28FAHVP-KV46F150MMIMXRT1015-EVK
FRDM-K64FHVP-KV58FMIMXRT1020-EVK
FRDM-K66FIMXRT1050-EVKBMIMXRT1060-EVK
FRDM-K82FLPC54018-IoT-ModuleMIMXRT1064-EVK
FRDM-KE02Z40MLPC54S018-IoT-ModuleQN908XCDK
FRDM-KE04ZLPC845BREAKOUTTWR-K21D50M
FRDM-KE06ZLPC8N04DevBoardTWR-K21F120M
FRDM-KE15ZLPCXpresso51U68TWR-K22F120M
FRDM-KE16ZLPCXpresso54018TWR-K24F120M
FRDM-KL02ZLPCXpresso54102TWR-K60D100M
FRDM-KL03ZLPCXpresso54114TWR-K64F120M
FRDM-KL25ZLPCXpresso54608TWR-K65F180M
FRDM-KL26ZLPCXpresso54618TWR-K80F150M
FRDM-KL27ZLPCXpresso54628TWR-KE18F
FRDM-KL28ZLPCXpresso54S018TWR-KL28Z72M
FRDM-KL43ZLPCXpresso55S69TWR-KL43Z48M
FRDM-KL46ZLPCXpresso802TWR-KL82Z72M
FRDM-KL82ZLPCXpresso804TWR-KM34Z75M
FRDM-KV10ZLPCXpresso812TWR-KV10Z32
FRDM-KV11ZLPCXpresso824TWR-KV11Z75M
FRDM-KV31FLPCXpresso845TWR-KV31F120M
FRDM-KW24MAPS-KS22TWR-KV46F150M
FRDM-KW36MCIMX6ULL-EVK-REV-A-6ULZTWR-KV58F220M
FRDM-KW41ZMCIMX7ULP-EVK-REV-BTWR-KW24D512
HEXIWEARMIMX8M-EVK-REV-BUSB-KW24D512
HVP-KE18FMIMX8MM-EVK-REV-CUSB-KW41Z

Components
adc_12b1mspsflexio_i2spit
adc_etcflexio_spiqtmr
adc12flexio_uartrit
adc16ftmrnga
aoigintrtc
cmpgpiortwdog
cmtgptsai
copi2csctimer
crcigpiosemc
csikppsha
ctimerllwusnvs_hp
daclpadcsnvs_lp
dcplpc_adcspdif
dmalpc_crcspi
dmiclpc_dmasystem
dspilpc_gpiotempmon
edmalpc_i2ctpm
eepromlpc_lcdctrng
elcdiflpc_rtcuart
enclpi2cusb
ewmlpsciutick
flexbuslpspivref
flexcanlptmrvspi
flexcomm_i2clpuartvusart
flexcomm_i2smcanwdog
flexcomm_spimrtwdog01
flexcomm_usartpdbwwdt
flexio_i2cpint