IAR compatible SDK for S32K328

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAR compatible SDK for S32K328

327 Views
ThiyaguK
Contributor I

Hello NXP Community,

I'm working on a project with S32K328 using IAR Embedded Workbench. I need help obtaining the proper startup files and linker configuration (.icf) for the S32K328.

Specifically, I'm looking for:

  1. Vector table setup for S32K328
  2. Startup code (cstartup_M.s equivalent)
  3. Low-level initialization code with proper register definitions
  4. IAR linker configuration file (.icf) for S32K328 memory layout
  5. Any S32K328-specific initialization requirements (ECC, cache, etc.)

I've checked S32 Design Studio but couldn't find anything concrete for S32K328 (attaching S32K328_Exmpl_IDE.zip) . I did find the startup and linker in the Platform plugins that came with MCAL (S32K328_RTD.zip). I am now confused which set of files to be used, any assistance, sample code, or pointers to resources would be greatly appreciated.

Thank you!

0 Kudos
Reply
0 Replies