TWR-K22F120M tower bootloader msd flash issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TWR-K22F120M tower bootloader msd flash issue

2,988 次查看
imx_proc_user
Contributor I

I flashed tower bootloader into the K22F120M board, K22 appeared as "FSL bootloader" folder on my host pc.  Board info is correct in the file INFO.TXT inside this filder:

Kinetis Bootloader K2.0.0

System device ID: 0x22001e99
Flash size: 524288 bytes
Flash range: 0x00000000-0x0007ffff
Flash sector size: 2048 bytes
Flash blocks: 2
RAM size: 131072 bytes
RAM range: 0x1fff0000-0x2000ffff
Reserved region 0: 0x00000000-0x0000dfff
Reserved region 1: 0x1fff0000-0x1fff25d7
Verify writes: yes
Check reserved regions: yes
Boot config present: no
Peripheral detection timeout: 0 ms
CPU clock: 48000000 Hz

 

The STATUS.TXT file says "Ready"

 

But when I drag the led demo led_demo_tower_20000.bin file into the folder, nothing is happenning. The STATUS.TXT file still says "Ready"

When I used the sb format (led_demo_tower_20000.sb), The STATUS.TXT file still says "Transfe". It looks like the file is transferring, but it hang forever.

 

The board file I used:

sources {
demo = extern(0);
}

section (0) {
erase 0x20000..0x7ffff;

load demo > 0x20000;

// jump to entry point
reset;
}

 

The BCA info is:

.section .bca, "a"

//__bootloaderConfigurationArea ; 0x3c0
// .long 'kcfg' // [00:03] tag - Tag value used to validate the bootloader configuration data. Must be set to 'kcfg'
.long 0x6766636b
.long 0xFFFFFFFF // [04:07] crcStartAddress
.long 0xFFFFFFFF // [08:0b] crcByteCount
.long 0xFFFFFFFF // [0c:0f] crcExpectedValue
.byte 0xFF // [10:10] enabledPeripherals
.byte 0xFF // [11:11] i2cSlaveAddress
.short 5000 // [12:13] peripheralDetectionTimeoutMs - Timeout in milliseconds for peripheral detection before jumping to application code
.short 0x15A2 // [14:15] usbVid
.short 0x0073 // [16:17] usbPid
.long 0xFFFFFFFF // [18:1b] usbStringsPointer
.byte 0xFF // [1c:1c] clockFlags - High Speed and other clock options
.byte 0xFF // [1d:1d] clockDivider - One's complement of clock divider, zero divider is divide by 1
.short 0xFFFF // [1e:1f] reserved
// Fill to align with flash configuration field.
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF // Reserved for user TRIM value

 

I am assuming that tower_bootloader will copy my led demo app into flash address 0x20000, and reset the board, then jump to the app. But it was not happenning. I am not sure what step I missed here. Please give me some advise! 

Thanks,

Jim

标签 (1)
0 项奖励
回复
3 回复数

2,592 次查看
imx_proc_user
Contributor I

It looks like that activePeripheral =0. msc_active = FALSE and hid_active=FALSE when called peripheral->controlInterface->pollForActivity().  

The USB and interface information is given in the BCA area. If the bca info is in the application image, and the application image is still in the host, how could bootloader read those info?  I think the bca should be part of bootloader, not part of the application

0 项奖励
回复

2,592 次查看
frankvanhooft
Contributor III

jimzhang wrote:

When I used the sb format (led_demo_tower_20000.sb), The STATUS.TXT file still says "Transfe". It looks like the file is transferring, but it hang forever.

Jim, did you ever solve this? I'm seeing the same thing on the KL25.

0 项奖励
回复

2,592 次查看
imx_proc_user
Contributor I

Sorry for the late response. I did not come back for a while. Did you s9olve the issue? My issue was that BCA direct mode flag was not set correctly.

0 项奖励
回复