Porting the KBOOT to K60F120M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting the KBOOT to K60F120M?

4,028 Views
naftalir
Contributor III

Hi,

 

How can i port the KBOOT to work with the K60F120M?

 

Thank you.

Labels (1)
Tags (3)
10 Replies

3,367 Views
mjbcswitzerland
Specialist V


Hi

For parts not supported in KBOOT there is an alternative to use the uTasker KBOOT compatible loader (UART, USB-HID and/or MSD, plus options for SD card, memory stick, Ethernet): http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

For the K60F120M see http://www.utasker.com/kinetis/TWR-K60F120M.html (no porting required)

Further potential benefits are smaller code size and greater IDE choice (CW, KDS, IAR, Keil, Atollic, Rowley, CooCox, Green Hills, GCC stand-alone and VisualStudio)

Regards

Mark
Kinetis for professionals: http://www.utasker.com/kinetis.html

0 Kudos
Reply

3,367 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

In the attachment, the Chapter 10 Kinetis bootloader porting has illustrated the whole procedure of Kinetis bootloader porting, so please refer to the attachment for details.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,367 Views
naftalir
Contributor III

Hi Ping,

Thank you for your reply but i cannot find the: "...NXP provides CMSIS-compatible packages for all Kinetis devices that contain bootloader-compatible device header files. These packages can be found on the product page for the MCU..." (quoted from the RM) K60F120 device header file, the closest device is : MK64F12 which isnt really works with the K60F120M.

how do i continue from the starting point?

where do i get the header files?

0 Kudos
Reply

3,367 Views
jeremyzhou
NXP Employee
NXP Employee

Hi naftalir,

Thanks for your reply.

I will appreciate if you can tell what IDE you use, then I can send the related startup and header files.

I'm looking forward to your reply.
Have a great day,
Piing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,367 Views
naftalir
Contributor III

Hi,

Please send me the correct files for K60F120M.

Im using IAR Embedded Workbench IDE (ver. 7.40.2.8570)

Thank you.

0 Kudos
Reply

3,367 Views
jeremyzhou
NXP Employee
NXP Employee

Hi naftalir,

Please check the attachment.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,367 Views
naftalir
Contributor III

 Im trying to follow the porting chapter with the files you provided me and with the K64FN1Mxxx12 icf file, but it seems to refuse running.

Do i need to change the icf file?Screenshot_2.png

Althogh, you attached the "MK60F12.h" file and i cant seem to find where to copy it and where do include it, it doesn't mentioned in the porting guide at all.

Thank you.

0 Kudos
Reply

3,367 Views
jeremyzhou
NXP Employee
NXP Employee

Hi naftalir,

In the fsl_device_registers.h, the related head files is included.

And the linker file needn't to be modified.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,367 Views
naftalir
Contributor III

Hi Ping,

I've tried with no success.

I've looked into the fsl_device_registers.h file but the MK60F12.h file isn't included there but the MK64F12.h, when i tried to comment it out and include the MK60F12.h file,  get many errors.

I've tried also to include them both: MK60F12.h and MK64F12.h in the fsl_device_registers.h file also got many errors.

When i compile the project with only the MK60F12.h file included, the compilation success but when i try to burn it i get an error:

Untitled.png

I use the J-Link programmer.

Thank you.

0 Kudos
Reply

3,367 Views
naftalir
Contributor III

Thank you!!

I will try that.. and of course will update this thread once it works :smileyhappy:

0 Kudos
Reply