MCUBOOT how to port to KE06XXX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUBOOT how to port to KE06XXX

1,279 Views
sunnywu
Contributor II

which similar target for MCUBOOT porting to KE06 should select,   I want to use the MCUBOOT 2.0.0 FOR project, but there is no target support for KE06xxx and KEAZ128XXX serials,   we want to select one similar targert for the porting,

I try to use the KV11, but I found it need modify more file contentes.  

0 Kudos
Reply
1 Reply

1,162 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi sunny Wu ,

   KE06 and KEA128 still don't have the KBOOT2.0 sample code for your reference.

   But, if you want to use the UART bootloader, actually, there has some application note about it:

https://www.nxp.com/docs/en/application-note/AN5400.pdf 

https://www.nxp.com/docs/en/application-note/AN4767.pdf 

   If you still want to use the KBOOT2.0, you need to refer to the KBOOT2.0 document, and migrate it by yourself.

https://www.nxp.com/webapp/Download?colCode=KBTLDR200RM&location=null 

Chapter 10 Kinetis bootloader porting

Wish it helps you!

Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply