KL03 bootloader DLL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL03 bootloader DLL?

1,317 次查看
andrewbarnes
Contributor I

I'm preparing for a KL03 design from our product dev group and I'm the guy who gets the production tools done.  We will be programming the uP in a production environment and from what I've found the serial boot loader is the way to go.  I will have a custom designed PCB for testing the product and I can easily add a serial port that the PC can use to program the KL03 directly but to do that I'd need a bootloader DLL and associated API documentation to make a PC app that talks to our internal database for programming parameters.  The other way is to code the boot loader into the uP on my custom PCB using the low level bootloader protocol documentation and use it to program the KL03.  The PC option would be much easier.  Is the DLL and API reference available and if so, where would I find it?

标记 (1)
0 项奖励
回复
1 回复

1,120 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

KL03 chip provides the ROM bootloader.

NXP provides the Kinetis Flash Tool, which is a GUI application on Windows® OS, aiming to offer the user an ease-of-use friendly user interface to communicate with the Kinetis device, running the Kinetis bootloader application.

This tool Supports Kinetis devices with Kinetis ROM bootloader, Kinetis flashloader, or running the flash resident
bootloader.

Customer could get this tool at [NXP_Kinetis_Bootloader_2.0.0 package] software, which could be downloaded from here.

The <Kinetis Flash Tool User's Guide> could be found with below path:

..\NXP_Kinetis_Bootloader_2_0_0\doc

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复