In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In device manager, USB on custom board for LPC54016 shows in "Universal Serial Bus Device"

3,449件の閲覧回数
NVazquez
Contributor IV

In device manager, USB on custom board for LPC54016 shows "LPC" in "Universal Serial Bus Device" instead of showing as "HID-Compliant vendor-defined device".

 

The Driver it is using is WinUsb Device. I don't think that is right and it should use hidusb.sys driver. The USB connector is connected to USB0 of the LPC54016. 

0 件の賞賛
返信
4 返答(返信)

3,426件の閲覧回数
NVazquez
Contributor IV

I tried with an HID example from SDK and I am able to see my board under "Human Interface Device" as "HID-Compliant device".

0 件の賞賛
返信

2,161件の閲覧回数
daihhqn
Contributor I

Could you please share me the HID? 

Thanks!

0 件の賞賛
返信

3,433件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I agree with that the PC should use the hidusb.sys driver for HID class.

BR

XiangJun Rong

0 件の賞賛
返信

2,162件の閲覧回数
daihhqn
Contributor I

Could you please share me official hidusb.sys to connect iMX6 devices

0 件の賞賛
返信