How small can the bootloader be? My target is 5K and I only need SPI.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How small can the bootloader be? My target is 5K and I only need SPI.

962件の閲覧回数
donwilley
Contributor II

I use a Kinetis MKL16Z32VFT4 that has just 32K of flash.  My present application takes up all but 5K of this, and while I might be able to shrink what I use now, I may also need to add more features, so let's say my bootloader is targetted to 5K with any application optimizations used to add features to the application.

The ideas I know about include:

- Reduce number of peripherals (bootloader_config.h changes).

- Reduce number of supported commands (bootloader_config.h changes). 

- Use newlib nano?

- Debug on systems with larger flash, but test 32k target with only release builds with size optimizations maxed out.

- Reduced use of libraries to use fewer, most basic options (for example puts() instead of printf() if practical).

- Find repeated code sections and make them functions.

- Evaluate code for flexibility I won't need.  Trim down functions that support options, parameters, and indirection that give great run-time flexibility but won't be needed in my application. 

It is an extreme example, but I might need just one kind of flash erase that starts at address 0x1400 and ends at 0x7FFF, so potentially the erase does need any parameters and other erase functions like erase all can be eliminated along with error codes/handling for invalid address range, protect/unprotect flash, etc.  

All suggestions welcome.

0 件の賞賛
返信
1 返信

779件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

You have done all I can imagine. But I think 5k is impossible on current code structure. Erase code is very small. You can't cut much meat from a skeleton.

Regards,

Jing 

0 件の賞賛
返信