Enabling spidev on ls1021a-tsn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling spidev on ls1021a-tsn

2,479件の閲覧回数
Raffaello
Contributor I

Hi all,

I am working on ls1021a-tsn board and I am interested to configure on board switch "sja1105". Due that I have compiled and sucessfully installed sja1105-tool and related libraries:

sja1105-tool --version
libsja1105 version: OpenIL-v0.3-201707
libsja1105 build date: Nov 11 2021 15:29:28
sja1105-tool version: OpenIL-v0.3-201707
sja1105-tool build date: Nov 11 2021 15:29:28

The problem is that when I call sja1105-tool (e.g sja1105-tool reset core)

the system answer is :

device_id field not defined in config file, setting default value 0x0
configuring device /dev/spidev0.1
can't open device
failed to open spi device.

On my board I find following files:

/sys/class/spidev
/sys/bus/spi/drivers/spidev
/sys/module/spidev

but i can't see spidev0.1 under /dev.

I think that the problem is related to device tree , but I don't know how to set dts file in right way.

 

Thank you in advacnce.

 

 

 

0 件の賞賛
返信
1 返信

2,465件の閲覧回数
Pavel
NXP Employee
NXP Employee
0 件の賞賛
返信