Bootloader SDK for S32K148EVB-Q176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader SDK for S32K148EVB-Q176

ソリューションへジャンプ
2,771件の閲覧回数
Chandra13
Contributor I

Hello,

  1. Is there a bootloader SDK available for the S32K148? I tried Select Board | MCUXpresso SDK Builder (nxp.com), but I could not find the specific configuration.
  2. For now, I use the Design Studio 3.4 to work on other topics (SPI, CAN, LIN). Do I need to download the MCUXpresso IDE to work on the bootloader topics?
0 件の賞賛
返信
1 解決策
2,762件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,763件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

0 件の賞賛
返信
1,631件の閲覧回数
CHYYDS
Contributor II

@Senlent Hello, do you have any information or documents related to bootloader for S32K344? Can you provide a link? Thank you very much!

0 件の賞賛
返信