sdk 1.3.0 exicution demo failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdk 1.3.0 exicution demo failed

2,326 Views
nandi_bhoopathi
Contributor I

Hi Team,

when we are trying to run a Vision sdk 1.3.0 exicution demo failed

isp_h264dec_single_stream.elf it is giving below errors.

** data/common/img_1280x960.h264 file will be used as input.
Press Ctrl+C to terminate the demo.
Framebuffer mapped at 0x7fa2313000.
Frame Wait timedout.
Demo execution failed.
data/common/img_1280x960.h264 file will be used as input.
Press Ctrl+C to terminate the demo.
Framebuffer mapped at 0x7fb8c8f000.
Sequencer other error:*** Sequencer error text:
FDMA queue full
../src/sdi.cpp: 1642/SeqEventHandler : [Error]: *** Other error message received.
../src/sdi.cpp: 1643/SeqEventHandler : [Error]: *** Sequencer error text:
../src/sdi.cpp: 1651/SeqEventHandler : [Error]: FDMA queue full
NULL pointer data.
Demo execution failed.
../../../../../libs/isp/sequencer/user/src/seq_user.cpp: 1044/SEQ_GraphStop : [Error]: Graph STOP failed: -1
../src/sdi.cpp: 1234/Stop : [Error]: Failed to stop the grabbing sequence.
Failed to stop the grabber.
Demo failed in cleanup phase.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,238 Views
nandi_bhoopathi
Contributor I

Any suggetions

0 Kudos
Reply

2,239 Views
nxf40536
NXP Employee
NXP Employee

Hi nandi.bhoopathi@craftlogiclabs.com‌. 

This looks like an SDK issue. Can you, please, upgrade to the newest Vision SDK ( 1.4.1 ) and see if you can reproduce your issue ?

0 Kudos
Reply