Hello everyone, I have already been able to configure the Matlab environment with the NXP.
But at the time I try to load the program "face_detection_camera_main" to the Board, I get the following error.
"C: \\ Users \\ waclab \\ AppData \\ Roaming \\ MathWorks \\ MATLAB" is not recognized as an internal or external command, program or batch file executable.
I have already tried adding the Path (as shown in the image) but in spite of that it does not work.
If you could help me, it would be very useful.