Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

3,504 Views
feng_shuo
Contributor II

Dears

What machine is fsl-image-ubuntu currently compatible with? Where can I see a list of compatible machines? Will fsl-image-ubuntu be compatible with s32v234sbc in the future? When will it be supported?

Thanks

Shuo

Labels (1)
0 Kudos
Reply
2 Replies

3,388 Views
Damienl
Contributor I


FSL is available ready to run for Mac OS X and Linux (Centos or Debian/Ubuntu) - with Windows computers being supported via the Windows Subsystem for Linux (WSL). We also provide source code if you run an OS not directly supported by us.

Tags (1)
0 Kudos
Reply

3,379 Views
Damienl
Contributor I

Thanks for this reply bp credit card

Tags (1)
0 Kudos
Reply