Hello,
I have a question about the datasheet of PTB36241G
I see the Vth(i) has two value: 75mV (min) and 150mV (max). It mean: The design has only one Vthreshold and it between 75mV and 150mV or the design has two Vtheshold, the signal will be detected when it > 150mV, and won't be detected when it < 75mV?
Thanks,
Chau
Hi chaunguyen,
This community is only for NXP Vision Matlab Toolbox.
We support all technical questions via a ticketing system. Please create a support request for this question at www.nxp.com/support using Support Requests option. This will ensure the correct answer from the subject expert.