Best option between S32V234-EVB2 and SBC-S32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Best option between S32V234-EVB2 and SBC-S32V234

2,250 Views
javiervicandi
Contributor II

Hi,

We want to start with the s32v234 to finally develop our own board based on this SOC.
Which kit do you consider the most appropriate considering the available information, schemes, etc?

S32V234-EVB2 or SBC-S32V234?

Thanks in advance

Javi

0 Kudos
Reply
2 Replies

1,052 Views
ronnena3
Contributor I

As i know the S32V234-EVB2 is a comprehensive evaluation board designed to showcase the capabilities of the S32V234 processor. It comes with various connectors, interfaces, and peripherals that can help you explore the features of the SOC. if you're looking for a comprehensive evaluation and exploration of the S32V234 SOC's capabilities, the S32V234-EVB2 evaluation board might be a better starting point. On the other hand, if you have a clear project in mind and need a more compact and focused development platform, the SBC-S32V234 single board computer could be a better fit.

0 Kudos
Reply

2,135 Views
Daniel_Popa
NXP Employee
NXP Employee

My recomandation is to use the SBC-S32V234

It is cheaper and developed in partnership with another company - hence more chances to get what you look for.

Best regards,

Daniel

PS: sorry for long delay. for some reasons we do not get notifications all the time about the threads.

0 Kudos
Reply