Question on freeMASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question on freeMASTER

3,329 Views
vpandey1
Contributor I

Hi there

I'm new to using freeMASTER & would appreciate if someone can help with following

1. How to use a command line to issue START command to freeMASTER to start with logging. For our test application running NI labview, command needs to be issued to freeMASTER to start the data logging. The unit under test is connected to PC through USB port and at power up embedded code will start with internal checks on unit & start outputting messages on USB com port. The power up is done using labview code.

2. Once data is logged need to save logged data to excel file. Please help on how to save data to excel file.

Thanks

Vinod

Tags (1)
0 Kudos
2 Replies

383 Views
kadanik
Contributor II
0 Kudos

3,278 Views
mariuslucianand
NXP Employee
NXP Employee

Hello vpandey@dynamiccontrols.com‌,

I think for your question you will find a proper answer on the FreeMASTER community space.

Hope this helps,

Marius

0 Kudos