vpp run on Lx2160ardb-rev2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vpp run on Lx2160ardb-rev2

1,541件の閲覧回数
Blue_Sky1
Contributor II

Hi Team,

I am using LLDPUG_RevL6.1.55-2.2.0,and build vpp used: bitbake vpp 

Machine : Lx2160ardb-rev2

vpp:v2302

dpdk:22.11

I found some problems:

    The vpp recognizes the created dpni and then configures the ip and mac addresses for this dpni.

    Then on the other host to this dpni traffic packets, when I use iperf to traffic a small flow of 2M, no problemBut when the traffic is slightly higher 5M, it quickly shows no buffer,and rx-miss。

     vpp(v2302) on  Lx2160ardb-rev2 whether to support the test of high traffic

     Or any suggestions for this test? vpp startup.conf is in the attachment.

 

stupid_0-1722414658600.png

 

1 返信

1,343件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

Would you kindly share the command, thanks

0 件の賞賛
返信