usb over-current condition on ls1021a board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb over-current condition on ls1021a board

Jump to solution
5,332 Views
MatthiasFuchs
Contributor II

Hi,

we ran into this issue on a ls1021a based custom board. Design is very similar to the

TWR board. But without the USB 3.0 hub.

During boot the linux kernel reports an over-current condition and port power is then disabled. So no USB devices are detected:

[ 3028.127516] hub 1-0:1.0: USB hub found

[ 3028.129991] hub 1-0:1.0: 1 port detected

[ 3028.143710] hub 2-0:1.0: USB hub found

[ 3028.146156] hub 2-0:1.0: 1 port detected

[ 3028.449817] hub 1-0:1.0: over-current condition on port 1

[ 3028.669099] hub 2-0:1.0: over-current condition on port 1

The kernel comes from the SDK 1.9 with only minor changes in its configuration.

The SDHC field in the RCW is set to 3 (for DRVVBUS/PWRFAULT). Our USB power switch is connected to these pins. DRVVBUS is low and PWRFAULT is high. That's the problem.

We changed the RCW[SHDC] to 1 so that the DRVVBUS can be controlled as GPIO. As GPIO we could enable DRVVBUS, the 5V were switched on and finally USB devices were detected.

So where does this over-current condition comes from? What might cause this strange problem?

USB does also not work in u-boot. But it does on the TWR board.

Matthias

Labels (1)
Tags (2)
1 Solution
3,496 Views
ufedor
NXP Employee
NXP Employee

The LS1021A PWRFAULT is an active high signal.

Please doublecheck the design to ensure that the signal polarity of the USB power switch is also active high. If not - external inverter has to be used.

View solution in original post

3 Replies
3,496 Views
brandensherrell
Contributor III

My stock ls1043ardb reports the same over-current error on boot with no configuration changes and no usb devices connected.

0 Kudos
Reply
3,496 Views
ufedor
NXP Employee
NXP Employee

Please provide a log with the RDB booting and the PWRFAULT testing.

0 Kudos
Reply
3,497 Views
ufedor
NXP Employee
NXP Employee

The LS1021A PWRFAULT is an active high signal.

Please doublecheck the design to ensure that the signal polarity of the USB power switch is also active high. If not - external inverter has to be used.