ubuntu mate cannot boot on ls1028ardb

cancel
Showing results for 
Search instead for 
Did you mean: 

ubuntu mate cannot boot on ls1028ardb

643 Views
540915622
Contributor III

I used the ubuntu mate file system generated by the following command of flexbuild_lsdk2004_update_290520

pastedImage_1.png

pastedImage_2.png

Labels (1)
0 Kudos
2 Replies

593 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 龙华 秦 ,

When you use ubuntu Mate filesystem, please connect the monitor to the target board.

Thanks,

Yiping

0 Kudos

593 Views
540915622
Contributor III

我接了DP接口的显示器。

我发现你们制作的ubuntu mate系统没有去挂载mmcblk1p2这个分区到/boot目录,然后没有将/boot/moudes目录软链接到/lib/moudes目录。你们的ubuntu main系统是有这些操作的,然后可以显示weston桌面。我手动执行上述操作后会成功显示ubuntu mate桌面。

我建议你通过flex-builder制作下ubuntu mate系统,然后烧录到板子上去看看就明白了。

当前flexbuild_lsdk有好多bug,你们什么时候更新?

0 Kudos