tftp boot of lsdk2004_ubuntu_main_LS_arm64.itb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tftp boot of lsdk2004_ubuntu_main_LS_arm64.itb

3,190 Views
karlgilkey
Contributor I
I used flex-builder to build lsdk2004_ubuntu_main_LS_arm64.itb 
I am able to tftp the file in uboot but I an error when the kernel boots. 

This is how I am attempting to boot:
setenv bootargs 'console=ttyS0,115200 root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 earlyprintk' 

bootp 0xA0000000 169.254.0.100:lsdk2004_ubuntu_main_LS_arm64.itb 
bootm 0xA0000000#ls1046afrwy 
This the output 
## Loading kernel from FIT Image at a0000000 ...
   Using 'ls1046afrwy' configuration
   Trying 'kernel' kernel subimage
     Description:  ARM64 Kernel
     Created:      2021-03-23  22:10:05 UTC
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0xa00000d0
     Data Size:    14083450 Bytes = 13.4 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x84080000
     Entry Point:  0x84080000
     Hash algo:    crc32
     Hash value:   5531a6c9
   Verifying Hash Integrity ... crc32+ OK
## Loading ramdisk from FIT Image at a0000000 ...
   Using 'ls1046afrwy' configuration
   Trying 'initrd' ramdisk subimage
     Description:  initrd for arm64
     Created:      2021-03-23  22:10:05 UTC
     Type:         RAMDisk Image
     Compression:  uncompressed
     Data Start:   0xa0d6e72c
     Data Size:    138956800 Bytes = 132.5 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00000000
     Entry Point:  0x00000000
     Hash algo:    crc32
     Hash value:   b76ff40c
   Verifying Hash Integrity ... crc32+ OK
## Loading fdt from FIT Image at a0000000 ...
   Using 'ls1046afrwy' configuration
   Trying 'ls1046afrwy-dtb' fdt subimage
     Description:  ls1046afrwy-dtb
     Created:      2021-03-23  22:10:05 UTC
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0xa922ea64
     Data Size:    31528 Bytes = 30.8 KiB
     Architecture: AArch64
     Load Address: 0x90000000
     Hash algo:    crc32
     Hash value:   d872df6c
   Verifying Hash Integrity ... crc32+ OK
   Loading fdt from 0xa922ea64 to 0x90000000
   Booting using the fdt blob at 0x90000000
   Uncompressing Kernel Image ... OK
   Using Device Tree in place at 0000000090000000, end 000000009001ab27
WARNING failed to get smmu node: FDT_ERR_NOTFOUND
WARNING failed to get smmu node: FDT_ERR_NOTFOUND

...

[    2.084255] Trying to unpack rootfs image as initramfs...
[    5.647102] rootfs image is not initramfs (read error); looks like an initrd
[    5.792695] Freeing initrd memory: 135696K
...
[    7.531828] RAMDISK: gzip image found at block 0
[    7.579631] RAMDISK: incomplete write (9263 != 9306)
[    7.584612] write error
[    7.598930] List of all partitions:
[    7.602432] 0100            4096 ram0
[    7.602433]  (driver?)
[    7.608535] 0101            4096 ram1
[    7.608535]  (driver?)
[    7.614634] 0102            4096 ram2
[    7.614635]  (driver?)
[    7.620738] 0103            4096 ram3
[    7.620738]  (driver?)
[    7.626836] 0104            4096 ram4
[    7.626837]  (driver?)
[    7.632953] 0105            4096 ram5
[    7.632954]  (driver?)
[    7.639058] 0106            4096 ram6
[    7.639059]  (driver?)
[    7.645170] 0107            4096 ram7
[    7.645171]  (driver?)
[    7.651273] 0108            4096 ram8
[    7.651273]  (driver?)
[    7.657412] 0109            4096 ram9
[    7.657413]  (driver?)
[    7.663518] 010a            4096 ram10
[    7.663519]  (driver?)
[    7.669719] 010b            4096 ram11
[    7.669720]  (driver?)
[    7.675915] 010c            4096 ram12
[    7.675916]  (driver?)
[    7.682101] 010d            4096 ram13
[    7.682102]  (driver?)
[    7.688300] 010e            4096 ram14
[    7.688301]  (driver?)
[    7.694486] 010f            4096 ram15
[    7.694487]  (driver?)
[    7.700689] 1f00          524288 mtdblock0
[    7.700690]  (driver?)
[    7.707223] 1f01           65536 mtdblock1
[    7.707224]  (driver?)
[    7.713769] b300        30326784 mmcblk0
[    7.713771]  driver: mmcblk
[    7.720576]   b301           23706 mmcblk0p1 661e76c1-01
[    7.720577]
[    7.727371]   b302         1048576 mmcblk0p2 661e76c1-02
[    7.727372]
[    7.734172]   b303        29188096 mmcblk0p3 661e76c1-03
[    7.734173]
[    7.740977] No filesystem could mount root, tried:
[    7.740978]  ext3
[    7.745854]  ext4
[    7.747776]  ext2
[    7.749692]  squashfs
[    7.751609]  vfat
[    7.753884]  fuseblk
[    7.755805]  btrfs
[    7.757982]
[    7.761473] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

Is there an issue with my bootarg? Why is this error happening.
0 Kudos
Reply
7 Replies

3,162 Views
karlgilkey
Contributor I

Thanks I have managed to build and boot ubuntu:lite and yocto:tiny.

I have tried adding additional packages to the file system of both images with no luck.

I need to add the nfs helper files. I tried to add nft-utils as an additon package. I don't see any change to the filesystem

In the end I also need to add Python3 as well. 

I added the packages to additional_lite_packages_list

and the local_arm64_tiny.conf but don't see a change. What do I need to rebuild.

 

0 Kudos
Reply

3,138 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please add "nfs-common" to "additional_lite_packages_list" in configs/ubuntu/additional_packages_list 

Then execute the following command.

$ flex-builder -i clean-rfs -r ubuntu:lite

$ flex-builder -i mkrfs -r ubuntu:lite

$ flex-builder -i packrfs -r ubuntu:lite

0 Kudos
Reply

3,126 Views
karlgilkey
Contributor I

So I am able to build and boot using buildroot:tiny.

How do I add packages to a buildroot filesystem?

When the build root image boots it does not bring up the network interface via dhcp. What do I need to change to get that to work on boot.

 

0 Kudos
Reply

3,110 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. add new “BR2_PACKAGE_NFS_UTILS=y” in configs/buildroot/qoriq_arm64_tiny_defconfig

2. rebuild it

$ flex-builder -i clean-rfs -r buildroot:tiny

$ flex-builder -i mkrfs -r buildroot:tiny

0 Kudos
Reply

3,132 Views
karlgilkey
Contributor I

I am runing flex-builder in a virtual box vm on a Windows 10 host.

When I run: flex-builder -i mkrfs -r ubuntu:lite 

It fails with this error.

gpgv: Good signature from "Ubuntu Archive Automatic Signing Key (2012) <ftpmaster@ubuntu.com>"
terminate called after throwing an instance of 'std::runtime_error'
what(): random_device::random_device(const std::string&)
qemu: uncaught target signal 6 (Aborted) - core dumped
/usr/local/bin/flex-mkdistrorfs: line 151: 7489 Aborted (core dumped) DEBIAN_FRONTEND=noninteractive DEBCONF_NONINTERACTIVE_SEEN=true LC_ALL=C LANGUAGE=C LANG=C apt -y update

I believe this is an error running qemu? Should I expect flex-builder to run in a VM? 

 

0 Kudos
Reply

3,174 Views
yipingwang
NXP TechSupport
NXP TechSupport

According to your following log, it seems that you didn't download the rootfs filesystem completely. As normal, the date size of ramdisk Image should be 600-700M.

   Trying 'initrd' ramdisk subimage

     Description:  initrd for arm64

     Created:      2021-03-23  22:10:05 UTC

     Type:         RAMDisk Image

     Compression:  uncompressed

     Data Start:   0xa0d6e72c

     Data Size:    138956800 Bytes = 132.5 MiB

     Architecture: AArch64

 

 You could regenerate the itb image with the following procedure.

$ flex-builder -i clean-rfs

$ rm packages/rfs/initrd/rootfs_lsdk2012_ubuntu_main_arm64.cpio.gz

$ flex-builder -i mkitb -r ubuntu:main -a arm64

In addition, the ubuntu:main rootfs is too large to run on LS1046AFRWY, you could use Ubuntu-based lite rootfs filesystem(Include Ubuntu 18.04 base packages and part of NXP's packages), it is about 180M, you could generate the itb image with the following command.

$ flex-builder -i mkitb -r ubuntu:lite -a arm64

0 Kudos
Reply

3,151 Views
karlgilkey
Contributor I

Now I am having problems build ubuntu:lite

I am running flex-builder in a virtual box vm instance of Ubuntu 18.04

When I try to run

flex-builder -i clean-rfs -r ubuntu:lite -a arm64
flex-builder -i mkrfs -r ubuntu:lite -a arm64

I goes all along and runs into this error. 

gpgv: Good signature from "Ubuntu Archive Automatic Signing Key (2012) <ftpmaster@ubuntu.com>"
terminate called after throwing an instance of 'std::runtime_error'
what(): random_device::random_device(const std::string&)
qemu: uncaught target signal 6 (Aborted) - core dumped
/usr/local/bin/flex-mkdistrorfs: line 151: 7489 Aborted (core dumped) DEBIAN_FRONTEND=noninteractive DEBCONF_NONINTERACTIVE_SEEN=true LC_ALL=C LANGUAGE=C LANG=C apt -y update

 

0 Kudos
Reply