reconfigure XIP mode to access bootflash for ls1043a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

reconfigure XIP mode to access bootflash for ls1043a

1,954 Views
lgx
Contributor I

my project use the ls1043a cpu, there are 2 qspi flashes, separated attached to cs0 and cs1.

cs0 flash is bootflash, run on XIP mode.  cs1 flash is data flash.

 

During bootup,  it will copy load_firmware.bin to run in OCRAM, responsible for loading firmware from data flash (cs1) and then return to bootflash.

 

After accessing data flash using AHB mode, how could i reconfigure QSPI controller to access bootflash in XIP mode ?

 

0 Kudos
Reply
8 Replies

1,932 Views
yipingwang
NXP TechSupport
NXP TechSupport

Investigating.

0 Kudos
Reply

1,871 Views
yipingwang
NXP TechSupport
NXP TechSupport

QSPI flash is XIP mode so based on the address scheme you define for your system, when you access back the bootflash address range, you will be in XIP mode.
Is there something I am missing? Please detail if yes.

0 Kudos
Reply

1,868 Views
lgx
Contributor I

Hi Yiping,

I am not sure about that. From my perspective, QSPI controller need to be setting to a special state to realize XIP access.

 

After i access the CS1 data sNOR, i need to configure the QSPI controller to AHB/IP mode to READ/ERASE/Program.   The qspi controller is not in the initial state (maybe bootROM configure for bootflash)

0 Kudos
Reply

1,694 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please provide more details on what issue is being faced.

Our RDB also has two flash and can be used for experimenting.

The QSPI flash is XIP which why it can be used as boot flash.

0 Kudos
Reply

1,633 Views
lgx
Contributor I
I have the similar requirements of "Multiple flash implementing RWW". cs0 is the boot sNOR, works on XIP mode, cs1 is the data sNOR.

https://www.nxp.com.cn/docs/en/application-note/AN12564.pdf

Do we have the demo logic to realize RWW on ls1043a ?
0 Kudos
Reply

1,605 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please create a new thread to address you new requirement?

0 Kudos
Reply

1,584 Views
lgx
Contributor I
0 Kudos
Reply

1,579 Views
yipingwang
NXP TechSupport
NXP TechSupport

Thanks a lot.

0 Kudos
Reply