Hi,
I am working on LS1046ardb Kit. When i am trying to boot from QSPI Bank0, D7 led is on which means that RCW is corrupted. How can i load rcw without using codewarrior ? Is it possible from Bank4 or sd card??
Both options are possible - please refer to the QorIQ LS1046A Reference Design Board Getting Started Guide, Table 11. Switch settings for boot sources.
For the SD card preparation please refer to the presentation "2018.06.12 Boot SD.pdf" in the following Community thread: