net-snmp AES128 decrypt issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

net-snmp AES128 decrypt issue

1,255 Views
Ghouse
Contributor V

Hi,

I have created snmpv3 user with privacy protocol AES128 and i can get the information using AuthNoPriv, but AuthPriv i am getting decrypt error.

snmpget v3 request as shown in screenshot.

please help asap.

0 Kudos
1 Reply

1,247 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether net-snmp package version is 5.1, this version doesn't support AES encryption.

Possible Cause: The SNMP device was unable to decrypt the SNMP V3 Read/Write request because the encryption passphrase and/or authentication styles do not match. Solution: Verify that the encryption passphrases and authentication styles set in the SNMP device configuration match those specified in the SNMP Driver's Device Properties. You need to add it in OpenSSL and check whether there is some issue with persistent snmpd.conf settings.

0 Kudos