Hi,
I want to use IXIA throughput to test performance on lx2160ardb_rev2 board.
Here is my architecture, and packets are send from IXIA port 0 to IXIA port 1.
IXIA port 0 -------- eth1 (dpmac.17) lx2160ardb_rev2 (dpmac.18) eth2 -------- port 1 IXIA
I found that even I have enabled ip_forward and not only pktgen but also ICMP packets can't be forward
from IXIA port 0 to IXIA port 1.
When I start throughput testing, only eth1 on lx2160ardb_rev2 can receive packets, it doesn't
forward the packets to eth2 on lx2160ardb_rev2 to send to IXIA port 1.
This situation is same when I use ICMP or pktgen to send packets from Host port 0 to send to Host port 1.
Host port 0 -------- eth1 (dpmac.17) lx2160ardb_rev2 (dpmac.18) eth2 -------- port 1 Host
ICMP packets and generated packets by pktgen are just received and not forwarded on lx2160ardb_rev2.
Here is the setting
lx2160ardb_rev2
eth1, 192.168.0.1
eth2, 192.168.1.1
Host
port 0 (eth0), 192.168.0.100
port 1 (eth1), 192.168.1.100
ip route add default via 192.168.0.1 dev eth0
What should I do to make the board to forward the packets?
Thanks.