lx2160ardb 2 memory sticks DDR controller 0 , no memory stick controller 1,cannot bootup,log :

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lx2160ardb 2 memory sticks DDR controller 0 , no memory stick controller 1,cannot bootup,log :

564 Views
ppbobo
Contributor I

There are 2 memory sticks on the DDR controller 0 on the lx2160ardb development board, and there is no memory stick on the controller 1, but it cannot be started.log :

INFO: Loading image id=31 at address 0x18003000
INFO: sd-mmc read done.
INFO: Image id=31 loaded: 0x18003000 - 0x180036d0
INFO: Loaded Imaged id 31 of size 6d0 at address 18003000
INFO: Execute firmware
INFO: 0x00240001: INFO: 0x3 INFO:
INFO: 0x04020000: INFO:
INFO: 1D Training failure
ERROR: Execution FW failed (error code -5)
ERROR: Calculating DDR PHY registers failed.
INFO: Time before programming controller 1536 ms
INFO: Program controller registers
PHY handshake timeout, ddr_dsr2 = 0
INFO: total size 32 GB
INFO: Need to wait up to 5920 ms
ERROR: Found training error(s): 0x100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platfor_def.h

0 Kudos
Reply
0 Replies