UBOOT下面 GPIO3[3]无法控制输出高低电平
1
RCW中加了2个配置项
IRQ03_00_PMUX=1
EVT43_PMUX=1
EVT20_PMUX=1
2 uboot中加了GPIO3[3]控制;
UBOOT加了段代码:
#define GPIO3_BASE_ADDR 0x2320000
u32 val = 0x00000008;
u32 tmp = 0;
readsl(GPIO3_BASE_ADDR, &tmp, 1);
val = val | tmp;
writesl(GPIO3_BASE_ADDR, &val, 1);
readsl(GPIO3_BASE_ADDR + 0x4, &tmp, 1);
val = 0x00000008;
val = tmp & (~val);
writesl(GPIO3_BASE_ADDR + 0x4, &val, 1);
readsl(GPIO3_BASE_ADDR + 0x8, &tmp, 1);
val = 0x00000008;
val = tmp & (~val);
writesl(GPIO3_BASE_ADDR + 0x8, &val, 1);
udelay(1000*20);
val = 0x00000008;
val = tmp | val;
writesl(GPIO3_BASE_ADDR + 0x8, &val, 1);
烧录启动后,发现GPIO3[3]一直都是0
3
uboot下手动操作
=> md.l 0x2320000
02320000: 00000008 00000000 00000000 00000000 ................
手动控制GPIO3[3]也无法控制
mw 0x2320008 0x8
返回还是
02320000: 00000008 00000000 00000000 00000000 ................
请问这个怎么办啊
谢谢!
Solved! Go to Solution.
Please refer to the following patches to make the MPC8XXX gpio driver to suppor fsl-layerscape platforms.
http://patchwork.ozlabs.org/project/uboot/patch/20200929092950.35372-1-ran.wang_1@nxp.com/
https://patchwork.ozlabs.org/project/uboot/patch/20200724110343.47079-2-hui.song_1@nxp.com/
https://patchwork.ozlabs.org/project/uboot/patch/20200724110343.47079-3-hui.song_1@nxp.com/
Please add "CONFIG_MPC8XXX_GPIO=y" in configs/lx2160ardb_tfa_defconfig in u-boot source code.
Please refer to the following patches to make the MPC8XXX gpio driver to suppor fsl-layerscape platforms.
http://patchwork.ozlabs.org/project/uboot/patch/20200929092950.35372-1-ran.wang_1@nxp.com/
https://patchwork.ozlabs.org/project/uboot/patch/20200724110343.47079-2-hui.song_1@nxp.com/
https://patchwork.ozlabs.org/project/uboot/patch/20200724110343.47079-3-hui.song_1@nxp.com/
Please add "CONFIG_MPC8XXX_GPIO=y" in configs/lx2160ardb_tfa_defconfig in u-boot source code.
1 when rebuild uboot, have building error as this..., add code, then can rebuild truely...
2 after program firmware to SD, re-power on, in uboot command, also can not control GPIO3[3]
3 Uboot log as this
md 2320000
02320000: 00000000 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320000 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320008 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 00000000 00000000 ................
02320010: 00000000 00000000 00000000 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320018 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320008 FFFFFFFF
md 2320000
02320000: ffffffff 00000000 ff0f8000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................
mw 2320008 0
md 2320000
02320000: ffffffff 00000000 00000000 ff0f8000 ................
02320010: 00000000 00000000 ffffffff 00000000 ................
02320020: 00000000 00000000 00000000 00000000 ................