Hi,
I am using lsdk20.04 for my development. The userland I selected is Ubuntu.
From the lsdk20.04 user guide, section 3.2 components I found following information:
Toolchain: gcc: Ubuntu/Linaro 7.3.0-16ubuntu3~18.04, glibc-2.27, binutils-2.30-0, gdb-8.1
I started my kernel with the ubuntu root file system(rootfs_lsdk2004_ubuntu_main_arm64.tgz). I checked the versions of following components:
Toolchain(ubuntu userland)
- gcc: Ubuntu/Linaro 7.5.0-3ubuntu1~18.04 (not 7.3.0)
- binutils: GNU Binutils for Ubuntu 2.30
- glibc: glibc-2.27
In Yocto sdk I can source an environment file
environment-setup-aarch64-fsl-linux
But If I want to do cross-compilation for ls1012ardb on my ubuntu 18.04 host machine. How could I set up the cross-compilation environment(set up the toolchain) for this case(ubuntu user land)?
Thank you!
Hello there.
I unable to find the toolchain at link fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.1.sh - Google Drive.
Please help.
Best regards,
Pratik
You could use Toolchain from Yocto 3.0 release, I uploaded it fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh - Google Drive .
$chmod 777 fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
$ ./fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
$ source /opt/fsl-qoriq/3.0/environment-setup-aarch64-fsl-linux
$ ${CC} hello.c -o hello
Hi Yiping,
Thank you for the quick reply.
Is it ok to cross-build packages for the ubuntu userland using the Yocto toolchain?
If I move to yocto sdk(3.1) and use yocto based tiny userland, could I get the Yocoto toolchain 3.1 from you? because I do not know where to get it.
I checked Index of /releases/yocto/yocto-3.1/toolchain/x86_64/ , didn't find the proper one for ls1012a.
Best regards,
Kai Wu
Hello Kai Wu,
I uploaded Yocto 3.1 Toolchain to fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.1.sh - Google Drive , please download it.
Thanks,
Yiping