lsdk flex-builder fails to build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lsdk flex-builder fails to build

1,146 Views
holder
Contributor I

I am using LSDK flexbuild1809 on Ubuntu 18.04 running in a VirtualBox VM.

My target is LS1088ARDB.

I run the following command:

flex-builder -m ls1088ardb -a arm64 -b sd

The build fails with the following error:

...

INSTRUCTION: mkbootpartition
DESTARCH: arm64
SECURE: y
CONFIGLIST: build_lsdk.cfg
INSTRUCTION: mklinux
DESTARCH: arm64
CONFIGLIST: build_lsdk.cfg
umount: /home/boeing/lsdk1809/flexbuild_lsdk1809/packages/rfs/ramdiskrfs/mntrd: target is busy.

I have to restart the build again which completes w/o error.

Any suggestions on the above "umount" error?

bob

Labels (1)
0 Kudos
Reply
2 Replies

816 Views
holder
Contributor I

I updated VirtualBox from 5.2.18 to 5.2.20.

I repeated the above build command and did not see the error.

0 Kudos
Reply

816 Views
Pavel
NXP Employee
NXP Employee

We use Ubuntu 18 Linux or Ubuntu 18 virtual VmWare machine for LSDK using.

There is no problem for building if Ubuntu 18 64bit is used.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply