Hi everyone,
I want to use wifi module(qca9984) over pcie. But i dont understand how to add it to device tree. I followed the https://elixir.bootlin.com/linux/v5.9-rc4/source/Documentation/devicetree/bindings/net/wireless/qcom... dts bindings but failed when pratice.
i open this configs in linux :
CONFIG_PCI=y
CONFIG_PICEPORTBUS=y
CONFIG_PCI_MSI:y
CONFIG_PCI_HOST_GENERIC:y
CONFIG_PCI_LAYERSCAPE:y
CONFIG_ATH10K:y
CONFIG_ATH10K_PCI:y
include "fsl-ls1088a.dtsi"
/ {
model = "LS1088A RDB Board";
compatible = "fsl,ls1088a-rdb", "fsl,ls1088a";
pcie@3400000{
status = "okay";
pcie@0 {
wifi@0,0 {
pinctrl-names = "default";
compatible = "qcom,ath10k";
reg = <0 0 0>;
qcom,ath10k-calibration-data = [00];
};
};
};
...
uboot log attached.
Solved! Go to Solution.
Device Tree node is required for the devices that cannot be discovered automatically, e.g. SoC integrated peripherals or devices connected via a simple bus. PCI is a plug-and-play bus which has special provisions for device discovery. For this reason, PCI(e) connected devices normally do not need to be declared in the Device Tree at all. If your device cannot be discovered using standard PCIe procedures, which is a rare case, consult at the device manufacturer ad/or the driver maintainer for required Device Tree node properties.
Have a great day,
Platon
Device Tree node is required for the devices that cannot be discovered automatically, e.g. SoC integrated peripherals or devices connected via a simple bus. PCI is a plug-and-play bus which has special provisions for device discovery. For this reason, PCI(e) connected devices normally do not need to be declared in the Device Tree at all. If your device cannot be discovered using standard PCIe procedures, which is a rare case, consult at the device manufacturer ad/or the driver maintainer for required Device Tree node properties.
Have a great day,
Platon