ls1043a using a 4.19 kernel with an uboot that uses PPA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1043a using a 4.19 kernel with an uboot that uses PPA?

1,521 Views
steven_vanden_b
Contributor I

Hello all,

We would like to use a newer bsp (like the freescale community bsp zeus edition) with the newer 4.19 kernel.

Since we already have devices deployed with the uboot and PPA installed on the boards, we would like to use the latest kernel but still be using the old PPA and uboot code on these devices.

Is this possible and is the log I have now indicating the issue with the PPA code?

It seems only the 1 cpu will start and the GIC cpu mask is not found, I assume this is because of the security software not loaded?

Greetings,

Steven Vanden Branden

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,421 Views
steven_vanden_b
Contributor I

I managed to solve the issues myself by using the original dts (and dtsi) files for the new kernel. Do i miss out on any fixes with regard to the buffers with the old dts files?

0 Kudos
Reply

1,421 Views
steven_vanden_b
Contributor I

It seems it is able to boot but the pca9553x driver is now segfaulting.

0 Kudos
Reply

1,421 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please diff the old and new dts files and provide the difference?

0 Kudos
Reply